사례 검색

검색 초기화
25개 중 21개 부터 25개 까지의 결과
Case banner
캄보디아의 환경과 지역 경제를 모두 살린 그런포스
Takéo Safe Water Supply teamed up with Grundfos to implement a well-tested technology – demand-driven distribution (DDD) – with a new financing model called a “Performance-Based Contract.”
캘리포니아 유기농 와이너리의 지속 가능성에 중요한 역할을 하는 펌프
Despite the otherwise brilliant growing conditions for grapes, Ampelos Vineyard in California's Santa Rita Hills does not get much rain. Therefore, Ampelos' irrigates its 46,000 vines from an aquifer 50 metres underground, brought to the surface with a Grundfos submersible SP pump.
펌프 시스템을 위기에서 두 번이나 구한 작은 상자 하나
Shortly after they installed their first Grundfos wastewater pumps and system, the crew at the Rose Creek Wastewater Treatment Plant discovered their usefulness. The MP204 motor protection units saved the plant from disaster one night - a problem that took minutes instead of
폐수를 자원으로 바꾸는 물 재사용
Previously, Grundfos disposed of used rinse water in the CED surface treatment plant at one of its factories. Now, the company treats it and reuses it onsite, saving water for both the factory and the community.
폴란드 최고로 거듭난 오래된 폐수처리장
Tomaszów updated its wastewater plant with a full-line supply of Grundfos pumps, mixers, optimised tank design and project execution. The city saved 50% energy and improved its water output to be among the best in Poland.