Grundfos sanitary pumps handle media with high viscosity

Overview_TEXT

개요

Nordzucker, based in Nordstemmen Germany, is a leading producer of sugar and a supplier of natural sweeteners. Their core business includes extraction and processing of sugar for the food industry as well as a wide variety of sugar products for the retail industries and for household use.

 

The situation
Before Nordzucker discovered Grundfos’ sanitary pumps, which are designed by Hilge, they were experiencing various problems, primarily due to the high viscosity of the sugar, which made it complex to process.

Nordzucker was looking to improve several parts of their sugar process, e.g. the process in which the liquid sugar was transferred through the system, the evaporation process throughout produc­tion, risk of crystallisation in the shaft seal due to the thickness of the sugar, etc.

 

The Grundfos solution
With Grundfos’ certified, sanitary, stainless steel product range, they were capable of helping Nordzucker ease the amount of problems they were experiencing throughout production.

Apart from the fact that the Grundfos sanitary pumps are highly reliable and repair and service friendly, Nordzucker strongly appreciated the unique hygienic design used, which would help reduce the time spent on cleaning. Furthermore, the mechanical sealing system available was valuable in order to ensure lubrica­tion, cooling and CIP capability.

 

The outcome
Today, 80% of the pumps for liquid sugar at Nordzucker are Grundfos sanitary pumps, such as Euro-HYGIA., Contra, MAXANA and SIPLA, which now all play an important part in the daily pro­cesses carried out at Nordzucker.

Nordzucker’s Technical Manager, Johannes Henze, comments, “The downtime has been reduced significantly and we are very pleased with our Grundfos pumps. Their service is fast and they are great at proposing solutions that fulfil our needs in the best way. Our experience tells us that compared with other pump suppliers Grundfos pumps have a higher quality in terms of effi­ciency, reliability and repair and service friendliness.

주제:

Grundfos sanitary pumps handle media with high viscosity

위치:

Nordstemmen Germany

회사:

Nordzucker

Pump

1. Gap-free seal areas
Corners and edges must be rounde off. Gaps, surface faults (cracks and scratches) must be avoided. Embossing and socket head screws should not be used.

2. Dead-end free pump casing

3. Shaft seal
Shaft seals are mounted in an optimum position in the product flow to ensure lubrication, cooling and CIP and SIP capability

4. Casing drain at lowest point

Related Products_TEXT